5G represents the next generation of wireless communications. But while the promises of 5G networks with higher capacity, lower latency, and increased bandwidth are exciting prospects, the value of such technological advancements will only be realized when they are applied to real-world use cases that drive mutual benefit to the end user. This is why engineers globally are endeavoring to unleash the benefits of 5G into a broad range of applications including gaming, virtual reality, autonomous cars, and wireless surveillance, to name a few. In each case, 5G is expected to drive innovative new business models, as companies start to take advantage of enhanced connectivity.
However, getting to the point of applying 5G at scale has predictably taken longer than some expected. Indeed, a recent survey commissioned by Molex and conducted by Dimensional Research showed that almost half of mobile carriers’ deployment plans have lagged compared to their initial expectations. The much higher signaling frequencies used with 5G have resulted in some unique engineering design challenges in areas such as signal propagation, power and thermal management, and antenna module placement.
Now, though, the efforts of engineers are starting to come to fruition, with 5G being rolled out around the world. The Molex survey showed that 89% of carriers were excited by the prospect of 5G, with 92% expecting to achieve their 5G business goal within the next five years. Furthermore, 99% of carriers said they expected 5G to deliver substantial benefits to end users within that timeframe. So, here, Molex makes a timely assessment of 10 critical technology enablers that go a long way to making 5G a reality.