In the OT world, we’re often dealing with data generated on the factory floor, perhaps related to the outcome of a manufacturing process. In many companies today, there is no path to get this data to the IT (enterprise) systems where it can be used in business decisions. With this disconnect, it’s difficult or impossible to process this data and convert it to meaningful information to monitor and react, in real time, to information such as yield, or any divergence from expected business outputs.
Historically, the technologies on the OT side are complex, and could have a direct impact on safety or environment, and hence need more maintenance than those within IT, and more attention from highly-trained staff. OT systems may be more constrained, networks are based on proprietary protocols (even if they claim to be open), or less user-friendly – while the IT side is less constrained and more flexible to adopt human centric designs and cutting-edge technologies. The direct ties and immediate impacts of IT on business outcomes have attracted very large investments on related technologies and contributed to drastic advancements in this field.
Another critical point to consider is security. Hacks, ransomware and malicious attacks are increasingly emerging as a major problem for all sorts of organizations, as shown by recent news stories. While there are many approaches to securing Industry 4.0 systems, the temptation is to leave the OT and IT parts separate, with an ‘air gap’ meaning that attacks cannot cross from one to the other. This spotlights another organizational challenge that must be understood and overcome to convince management that the benefits are worth the extra cost of a unified yet secure approach.
If we look briefly at the enabling technologies for unifying IT and OT, networking and communications are always important. OT systems often use relatively old protocols with no security provisions, while the IT world relies on secure infrastructures. Ethernet is an excellent solution for many needs, but it is not enough for all OT applications as it doesn’t provide the real-time, guaranteed low latency performance needed on the factory floor. Recent developments, such as time sensitive networks (TSN), are addressing this issue converging the IT/OT networks, and broadening the scope of Ethernet applications, but there is still a long way to go to enable true unification.
Other technologies are taking on important roles to drive IT/OT unification, such as IP-enabled process controls, networked sensors, and secure public and private clouds for data storage. Standardization is being enabled by new initiatives, such as Open Platform Communications Unified Architecture (OPC UA), and Industry 4.0 is one of the key applications for new 5G communications networks.