There is little doubt that the future holds a very different automobile from those on our roads today. It will almost certainly be fully self-driving in most, if not all, situations by the time all is said and done. In fact, the Society of Automotive Engineers (www.sae.org) has published a well-defined roadmap that outlines the six stages of the evolution, leading to fully autonomous vehicles at Level 5.
But what are the hurdles to the realization of the promised end game? To achieve a driverless future, there are a multitude of technical challenges to overcome in all aspects of the vehicle design. For example, the control system challenges in a driverless car revolve around such matters as safety, security, and standards. But the technical trials pale in comparison to the ethical and moral questions that arise when developing these systems. What will the vehicle do when it is faced with an unavoidable accident? It’s just a case in point in a field of similar quandaries – a modern version of the classic trolley paradox.