Industrial Automation (AI) is at an inflection point. Organizations around the world are well on the way to implementing the technologies that allow them to realize the promise of Industry 4.0. Indeed, the recent State of Industry 4.0 Survey conducted by Molex, determined that 87% of respondents are excited about the transformative power of Industry 4.0 over the next decade. But how do organizations develop smart ways to leverage these advancements as machines leap forward in intelligence and capability?
The IA supply chain—from robot manufacturers to complex machine builders and systems integrators to line constructors—is well positioned to move forward to the machine intelligence future that will make Industry 4.0 a reality, with nearly 70% of respondents optimistic that it will help them build better products. Yet there are still some obstacles to overcome, such as the separation of IT and OT, and communication protocols that are too limited, translating to legacy infrastructure and associated investments slowing down the transformation.
To achieve an effective transition to Industry 4.0, organizations must modify existing unwieldy IA command structures to deliver greater flexibility, a more free flow of communications, and smart connectivity across an open, scalable and connected platform that taps into the full power of Industry 4.0 technologies.