There’s much debate and discussion about whether single-ended or differential cabling/connector solutions are best positioned to address system architecture and performance needs. I led a deep-dive discussion on this topic at the Automotive SerDes conference in October, offering insights and perspectives.
Making the choice between single-ended (i.e., coax cables are terminated with coax connectors on both ends of the cable) or differential (i.e., shielded twisted pair or shielded parallel pair with fully shielded differential connectors on both ends of the cable) strictly depends on the application. The challenge in picking the best approach is complicated by the growing number of applications with different protocols, which increases wiring, complexity and weight.
A general distinction between single-ended and differential cables is that the latter sends a signal over two cable conductors while the single-ended uses one. The pair of conductors enables opposite polarity to cancel interfering signals from the environment. There also are several types of differential cables. Shielded twisted pair (STP) helps suppress noise with the twisted conductors’ construction while shielded parallel pair (SPP) refers to two conductors that are parallel to each other for the most part, which enables better IL performance due to physical length benefits resulting from the reduction in twisting.
Shielded twisted pair (STP) helps equalize and suppress noise while shielded parallel pair (SPP) means the two cable strands are straight.
There are variants for the cable shielding too, and the material from which the cables are made is also relevant. The subsequent placement within the vehicle also should help determine the material. For example, if a cable is installed in a door that frequently is opened and closed, it must be flexible. For example, if a cable is located in the engine compartment, the temperature rating of the cable assembly must be updated to 125 degrees Celsius. In general, while differential cables are better at suppressing background noises, they are more expensive and heavier than single-ended alternatives.
To better understand where people stand on this topic, I posed a question to the SerDes conference attendees about which approach was poised to win in the long run. Interestingly, the majority chose differential cabling for the biggest growth potential in the future.