Tomorrow’s market disruptors and technology codebreakers are working hard to decipher what mobile devices will look like in the future and how they’ll perform differently than today’s counterparts. Will they be bigger, smaller, lighter, handheld, worn or implanted? Which big-bet innovations will yield the biggest payoffs? And which barriers will take the longest to remove?
These questions and many more were posed to more than 200 mobile-device manufacturers and suppliers in The Future of Mobile Devices global survey. Commissioned in July, this latest Molex survey examined the features and enablers expected to guide the development of mobile devices to be built within the next five years. As most manufacturers are already developing their 2023 models, mobile devices manufactured in 2026 might look and operate like current models. Still, game-changing innovations are accelerating rapidly, so there are high expectations we’ll see an altered landscape in a relatively short period of time.
According to the survey, a wide range of disruptive features are anticipated to become standard by 2026. Participants prioritized self-charging or energy-harvesting capabilities (37%); holographic or projection displays (36%); fully recyclable (32%); environment-proof, such as dust- or waterproof (31%); and no-break displays (29%). All of these represent current investment areas, so it’s feasible to expect continued development without conjecturing whether, or if, they will become standard in five years.
Nearly everyone (90%) also believes continued evolution in form factors will alter tomorrow’s mobile devices, yet no consensus was reached on a preferred form factor. While 35% predict dramatically different user experiences (e.g., glasses, watch or other wearables), another 32% expect similar user experiences from slightly different form factors, such as foldable or rollable devices. Finally, 23% of those surveyed don’t expect drastic changes—even if form-factor sizes increase or decrease.