Although often hidden from view, there can be no debate that our reliance on data centers is spiraling. In their report ‘Data Age 2025’, analyst firm IDC forecasts that within four years, society will generate 175 zettabytes (ZBytes) of data each year – somewhere between two and three times the current rate. The report goes on to suggest that there will be 6 billion connected users by that time, each of whom will interact with a data center almost 5,000 times per day – triple today’s rate and 10 times what it was in 2015.
Cloud-based services are increasing, especially via mobile devices and billions of IoT nodes, which further heightens the reliance upon data centers. In the past, data centers were used primarily for storing data, and access time was not critical. However, today, a low-latency operation is becoming the ‘norm’ to support high-demand applications and capabilities such as voice assistants and video streaming. With the rapid changes in the data landscape comes the new definition for key attributes of the modern data center, with flexibility, adaptability, scalability, and reliability all rising to the top. And all point a spotlight on the need for efficiency.
As the energy consumed by data centers inevitably rises, efficiency in data centers has become not just desirable but critical. In November 2018, the International Energy Agency estimated that data centers consume 1-1.5% of the world’s energy in their report entitled ‘Digitalization and Energy’. While efficiency improvements ensure that energy usage does not rise in exact proportion to data, clearly data centers have the potential to become even more significant energy users in the near future.
Organizations building their own data centers (or relying on a partner to do so) are facing unprecedented energy-related challenges. Many are adopting a range of measures to regularly monitor their performance, with PUE (Power Usage Efficiency) being very common. This measures how much of the total power consumed is used for powering IT equipment and how much is used for other infrastructure, including battery management, UPSs, and cooling. Essentially, PUE challenges data centers to use as little energy as possible on activities that don’t add value.