Over the past decade, modern technology has propelled efficiency enhancements at an exponential rate—even reducing the amount of effort required to interact with everyday staples like thermostats, appliances and entertainment systems. What used to involve the press of a button or turn of a knob now entails the subtlest touch of a finger, all thanks to the innovative functionality of capacitive switches and conductive sensors.
This revolution is largely being driven by today’s consumers, who increasingly prefer to manage personal productivity tasks via single-tap smartphone applications. It’s an efficiency trend that’s also overtaking the home appliance market, with demand for internet-connected home appliances continuing to rise. Statista currently projects that over 57% of U.S. residences will include at least one smart home device by 2024, and Grand View Research expects the global smart home appliance market to expand at an 8.6% compound annual growth rate from 2022 to 2030. At the same time, governments and consumers continue to push for more environmentally friendly designs and energy-saving sustainability.
As these developments intensify the spotlight on smart home appliances and their human-machine interfaces (HMI), Molex remains at the forefront of recent advances. One prime example: We’re helping today’s manufacturers create a variety of modern HMI more quickly and easily than ever, by leveraging the power of PEDOT—an acronym that stands for polystyrene sulfonate or poly (3,4-ethylenedioxythiophene). This new, groundbreaking technology is changing the game in intelligent appliance design.