Zonal architecture could have a major impact on vehicle production, accelerating innovation and speeding the delivery of adaptive controls and safety features. But to succeed, it will require high-speed data connections that are flawless, robust and keep data flowing securely.
That’s not easy to achieve in vehicles that are exposed to wind, rain and constant shock and vibration. These conditions pose challenges for electronics, especially within lines carrying high-speed data.
The growing number of sensors and cameras in advanced driver assistance and autonomous systems will generate unprecedented amounts of information that must be processed at high speeds. If vibration causes even a momentary break in a connection with data speeds of over 1 Gbps, large amounts of information could be lost. With safety controls becoming more automated, it is imperative to build connectors that are capable of overcoming vibration risk.
Connectors in the central computing cluster will also need to provide far greater resilience than conventional board-to-board solutions while also offering high pin counts and power connections. Engineers plan to standardize their designs to allow swappable modules, simplifying the manufacturing processes and allowing for easy upgrades.
Molex is working closely with manufacturers and Tier 1 suppliers, leveraging its world-class signal integrity capabilities to create a new generation of hybrid and mixed connectors that can successfully carry both power and high-speed signals in harsh road conditions. In addition to improving reliability and safety, the new connectors will make installation easier since their combined functionality will result in fewer connection points.
At the same time, Molex is building on its expertise in microminiature connections from applications like smart phones to enable tiny, high-bandwidth board-to-board attachment everywhere from the central computer to camera modules. Ultimately, it’s all about bringing efficiency to every aspect of the next-gen EV architecture.