In fact, Molex’s collaborative approach extends to our customers and our suppliers. Over time, these collaborations have evolved into deep relationships, expanding our role as a strategic technical advisor.
In the case of the Quad-Row micro connector, Molex engineers identified that SMT service providers use a standard 0.35mm pitch for ease of manufacturability. Anything smaller than 0.30mm pitch is currently difficult to efficiently and accurately assemble and process. To maintain manufacturability and assembly confidence with CMs, Molex engineers determined the familiar layout for the mounting pads needed to remain intact. Instead, the team focused on what it could control: the internal signal contacts layout.
In collaboration with experts from a global leader in design, development and manufacturing of FPCs the Molex engineering teams determined that staggering the pins as close as possible allowed the pins to be positioned across four rows at a much closer signal contact pitch of 0.175mm. The result: the first ever staggered circuit layout that delivers unprecedented space savings of 30% – enabling high-density circuit connectivity.
This was all made possible through consistent teamwork and Molex’s engrained dedication to forming strong relationships with its customers and supplier ecosystem. By establishing advocates within the R&D department of the FPC supplier, the engineering team was able to persuade the FPC supplier and the smartwatch manufacturer to make key design changes—such as soldering the micro connector to the FPC. This changed the game in terms of design, opening up key opportunities for more capabilities to be tucked into a tighter space. Molex design engineers also assessed that the design change would also improve reliability when manufacturing at scale.