Molex Road Noise Cancelling (RNC) Sensors are designed to meet the stringent needs of various harsh environments. Our exterior- mounted sensors, such as the RNC Sensors, are design for an IP6K9K rating according to the ISO20653 specification, salt mist/water exposure, and impact loading, making them especially suited for the underbody mounting conditions.
The Molex family of accelerometer sensors are designed around low noise floor accelerometers that enable them to sense a lower energy level vibration or movement. This correlates to the accelerometer sensing vibration noises at very low speeds of vehicle movement. The yellow blocks in the following image show the region of the wave form that would not be captured by other accelerometer technologies.