Automating the design process, such as using EDA tools to develop integrated circuits, leans heavily on design reuse. This typically takes the shape of proven functions that are packaged up to become ‘building blocks’ that can be slotted together to create a complete solution.
The metaphor can be extended to describe how the building blocks enable each layer of integration in the product design process, and even further to define how the final product may be manufactured using those components and sub-systems which, themselves, become building blocks.
This is where having the ability to design product and manufacturing platforms that are building blocks for multiple generations of product can deliver substantial gains in the design and manufacturing process and maximize the efficient use of scarce resources. Molex follows this ethos when working with customers and their design experts to develop new ‘building blocks’ that meet the end product’s requirements exactly.
Across its optical solutions business, Molex uses collaborative design tools with its customers to propose initial concepts for optical module products. Beyond the technical performance parameters, we can address size, configuration, connection interfaces, and aesthetics. The full module is simulated so that we can predict performance and create advanced features before making the first physical parts. The tools allow engineers to position fully architected products in a 3D environment as working examples within the customer’s end application, using animation to demonstrate how the product will fit, interact, and function. Customers benefit by seeing results quickly and having the opportunity to provide input, enabling Molex to respond rapidly with change requests and enhancements that make the product development cycle more efficient.
In concert with its advanced design capabilities, Molex also uses advanced manufacturing capabilities and technology innovation to automate our advanced optical wavelength switches using our optical fabric-build automation robotics platform. Aligning optical lightpaths for clear transmission is key to reliable performance in communications systems. The final alignment of the optical system is achieved via automated robotic control. Molex custom alignment stations optimize the degrees of freedom that light can travel. We develop custom software to monitor light running through the optical circuit to control the robotic alignment of all the various elements. Not only does this result in better products that can be built more efficiently, but it ensures better uniformity from unit to unit and across operators and manufacturing processes.
Designing our products with the technology to apply advanced manufacturing methods at the early stage of product design allows us to work with our customers and factory teams to work on streamlined manufacturing, even before the first pilot runs of the product on actual equipment is finalized.
Once in volume production, Molex employs advanced automation using robotics and computing capability to monitor the health and efficiency of our production lines in real-time. This allows changes with minimal interruption to production, thus increasing throughput and minimizing downtime. Ultimately, this combination of advanced technology in design and manufacturing enable Molex to respond with greater speed and create more value for customers, suppliers, and society.