Skip to main content
alt text

QSFP-DD800 MSA Group Annouces Initial Hardware Specification

Mar 06, 2020

SAN DIEGO - On the heels of its 2019 debut, the Quad Small Form Factor Pluggable Double Density 800 (QSFP-DD800) Multi Source Agreement (MSA) group today announced the release of a new hardware specification for the QSFP-DD800 transceiver form factor. The MSA group was formed to advance the development of high-speed, double-density QSFP modules which support 800 Gbps connectivity and includes the following promoters: Broadcom, Cisco, II-VI, Intel, Juniper Networks, Marvell, Molex and Samtec.

The QSFP-DD800 MSA is focused on the next generation of the QSFP family of modules. The new QSFP-DD800 1.0 specification is intended to be incremental to the existing QSFP-DD 5.0 specification. As signal integrity and thermal performance remain imperative, the transceiver pads have been optimized to improve signal integrity for 100 Gbps performance per lane without affecting backwards compatibility. The new specification additionally defines a novel 2x1 connector/cage, with cabled upper ports as an option to address signal loss issues associated with tradition PCBs. Looking ahead, QSFP-DD800 promoters will continue to work on new connector/cage variants, including 2x1 SMT versions that operate at 100 Gbps per lane.

“In the short time our group has collaborated, we are thrilled to introduce this first specification for the next generation of the QSFP family of modules,” said Scott Sommers, co-chair of the QSFP-DD800 MSA. “As signal integrity and thermal management remain challenges for the optical communications industry, our MSA group is confident that its solutions will meet performance needs.”

“With their superior system integration and design flexibility, QSFP modules continue to be the cornerstone in building next generation networks and network equipment, especially as port speeds increase to 800G,” said Mark Nowell, co-chair of the QSFP-DD800 MSA. “Furthermore, their ability to increase switch and routing bandwidth density without sacrificing backwards compatibility with QSFP-DD, QSFP56 and QSFP28 modules provide network operators tremendous commercial and operational advantages.”

The QSFP-DD800 MSA group is also announcing that it will act as an incubator, collaborating with the QSFP-DD MSA, to provide specifications to that group with the intention of it being included within the QSFP-DD specifications. Therefore, companies interested in joining and participating in QSFP-DD800 development are encouraged to join the QSFP-DD MSA.

For more information on the QSFP-DD800 MSA please visit www.qsfp-dd800.com.

Caution Concerning Forward-Looking Statements
We are disclosing forward-looking information so that investors, potential investors, and other owners can better understand the mentioned Companies’ future prospects and make informed investment decisions. The information in this press release contains “forward-looking statements” within the meaning of the Private Securities Litigation Reform Act of 1995. These statements can be identified by the fact that they do not relate strictly to historical or current facts. Any forward-looking statement made by the Companies speak only as of the date on which it is made. The Companies are under no obligation to, and expressly disclaim any obligation to, update or alter their forward-looking statements, whether as a result of new information, subsequent events or otherwise.

Share

 

About Us


Molex is a global electronics leader committed to making the world a better, more-connected place. With a presence in more than 40 countries, Molex enables transformative technology innovation in the automotive, data center, industrial automation, healthcare, 5G, cloud and consumer device industries. Through trusted customer and industry relationships, unrivaled engineering expertise, and product quality and reliability, Molex realizes the infinite potential of Creating Connections for Life. 

Learn More About How We Create Connections for Life