| Customized | Cell Types | Standards |
|---|---|---|
| Designed to meet customer’s requirements | Prismatic and Cylindrical | Automotive |
Features and Benefits
Manufacturers are looking for decreased labor time and reliable battery cell connections. Molex addresses this challenge through the FPC/PCB/FFC connectivity of the Volfinity system that eliminates the need for daisy-chain wiring. As a result, battery module customers can expect a more reliable solution from the FPC connection as it eliminates human errors in manual wired connections. Additionally, FPC connectivity is more resilient to degradation when compared to wires.
Commercial vehicle manufacturers need large, powerful batteries while simultaneously meeting weight requirements. The thermoplastic carrier, lamination and thermal forming in the Volfinity system are relatively lightweight while delivering a reliable connection through the high voltage sensing connection. As a result, the Volfinity system is an attractive solution for commercial vehicle designers who need to maximize battery capacity while keeping modules as light as possible.
Manufacturers also seek highly compact electrical connections which are addressed by the Volfinity Cell Contacting System. This system provides a space-optimized and integrated cell sensing board, which is designed to fit within tight spaces effectively. As a reliable electronic board solution, the Volfinity Cell Contacting System simplifies sourcing and enhances performance across applications such as energy storage systems, commercial vehicles and industrial applications.
Featured Videos
Volfinity Cell Contacting System
The all-in-one design of the Volfinity system combines in-house design, production and outsourced resources like busbars and connectors to simplify supply chain logistics, while eliminating the need for daisy-chained wires. This system provides a direct, reliable interface solution connecting each battery cell directly to the control board by using an FPC connector, which reduces wiring complexity, minimizes resistance and voltage drops, improves safety by reducing heat generation and enhances system reliability. The Volfinity system is customizable to meet different customer requirements and also supports next-generation thermal and electrical performance needs for evolving technologies.
Applications by Industry
Electric loaders
Electric mowers
Electric tractors
Electric vehicles
Grid energy storage
HVAC energy storage systems
This is not a definitive list of applications for this product. It represents some of the more common uses.
Frequently Asked Questions
How does Molex determine the size and shape of the busbar used in its Volfinity system?
Molex engineers analyze the optimal form and shape of the aluminum busbar to meet thermal, electrical and mechanical performance requirements.
How does Molex weld the FPC connector to the aluminum busbar?
Molex engineers determine the optimal weld profile for similar and dissimilar materials to the aluminum busbar in order to ensure a reliable electrical and mechanical connection.
Does Molex manufacture the FPC connector used in the Volfinity system?
Yes, Molex offers various interconnect options required for the Volfinity Cell Contacting System. These options are part of Molex’s portfolio of reliable connectors, including the Flexi-Latch and Float Stack connector systems, which simplify the customer’s procurement process.