Skip to main content

Zonal Architecture: Making the Car of the Future Possible

The advantages offered by zonal architecture will change the automotive design completely. At its heart, the zonal approach reduces the complexity required of the cable harnesses within the vehicle, both in terms of the number of wires and the distances they are required to travel.

Download the Whitepaper

Overview


In contrast to a domain architecture in which vehicle systems are grouped by function, zonal architecture offers a more efficient solution. The functions within a vehicle are grouped by location into several zones. Each zone is responsible for the devices that are installed in a particular section of the vehicle and are connected to a locally installed zonal controller or gateway. Because a zonal gateway is close to the devices it controls, the cable lengths required to connect them are relatively short.


Blog

Zonal Architecture vs. Domain Architecture

Discover why automakers are migrating from domain architecture to zonal architecture to support the functionality of tomorrow’s vehicles. Read to learn more.  

Connecting the Zones

Connectors will be critical to these designs, and Molex is already collaborating across markets and business units while leveraging its world-class signal integrity capabilities to deliver both high-power and high-speed solutions in this new automotive environment.

Download the Infographic

MX-DaSH Data Signal Hybrid Connectors

MX-DaSH Data Signal Hybrid Connectors combine varying automotive signal terminals in one connector system, delivering a compact connectivity solution for a range of automotive applications requiring reliable data transmission.

Additional Resources


BLOG

Five Revolutions in Vehicle Design

Zonal architecture is ushering in a new era in vehicle electronics design. Grouping functions of the vehicle by location zones with each zone being responsible for the devices that are installed in a particular section of the vehicle, zonal connections must be made through a locally installed zonal controller or gateway.

Image

BLOG

Automotive Innovations Paving the Way

The automotive industry is one of the most exciting and dynamic segments of technology today. With so many innovations maturing simultaneously, the architecture and design of the car of the future are poised to change forever.

BLOG

Vehicle Architecture: The Innovation Turning Point

The automotive industry has a long history of embracing new technology. Each generation of cars and vehicles becomes more advanced as manufacturers introduce new features that improve safety, efficiency and passenger comfort.

BLOG

The Data Center on Wheels Speeds into View: Envisioning the Future of Automotive

The automotive industry is transforming rapidly, impacting next-generation vehicle architectures, driving experiences, partner ecosystems and production manufacturing. Increasingly, tomorrow’s cars and trucks will embody the traits and technologies of powerful computer systems fueled by software, storage, connectivity and computing—essentially performing like a “data center on wheels.”


MX150 Connectors

Mini-Fit Connectors

DuraClik Connectors

PRODUCTS FOR VEHICLE ARCHITECTURE

Explore innovative products backed by engineering excellence and Molex's commitment to quality and reliability to inspire the development of vehicle architecture.

   Sealed Option   Wire-to-Board   Wire-to-Wire   Board-to-Board
CMC/CMX  X X    
ConnTAK50   X    
DuraClik X X    
Easy-On   X    
EdgeLine       X
HD Mezz       X
HFM X X    
HSAL1   X    
HSAL2 X X    
Mini50 X X X  
Mirror Mezz       X
Mizu-P25 X   X  
Mizu-P38 X   X  
MX64 X   X  
MX123 X X    
MX150 X X X  
MXP120 X   X  
SEARAY       X
SlimStack       X
Stac64   X    
stAK50h   X    
V1 Appliances